AXIS#.LOAD.INERTIA

Description

AXIS#.LOAD.INERTIA sets the load inertia.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

1 to 1,000,000 kgcm² or kg

Default Value

0 kgcm² or kg

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.LOAD.INERTIA

5014h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.LOAD.INERTIA

5114h

01h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.LOAD.INERTIA

5700

1644

Unsigned32

Read/Write

-

AXIS2.LOAD.INERTIA

71236

1164

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.LOAD.INERTIA

5700

Float

Read/Write

-